5G NR

Rate Match Pattern Editor DL

Add Pattern

Remove/Delete Pattern

Copy Pattern

RateMatchPattern Count

ID

Enabled

Level

Subcarrier Spacing

RB Index

Symbol Bitmap Span

Symbol Bitmap

Periodicity

Periodicity Pattern Bitmap

Add Pattern

Adds a new RateMatchPattern row to the table with default values. Up to 8 rate match patterns can be used.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > + sign to Add

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern:ADD

SCPI Example

 

Couplings

If count of Rate Match Pattern is 8 and try to add a new Rate Match Pattern, error -224 "Illegal parameter value; Failed to add Rate Match Pattern because limit of 8 has been reached." will be shown.

Initial S/W Revision

A.09.00

Remove/Delete Pattern

Removes the currently selected RateMatchPattern row from the table. The remaining patterns will be re-indexed.

Clicking this button when there is only one RateMatchPattern row in the table displays a message stating, "The last RateMatchPattern can't be removed, you can set it to off to disable it."

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > Ellipsis icon > Delete

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern:DELete <integer>

SCPI Example

 

Couplings

If the Rate Match Pattern to be delete does not exist, error -224 "Illegal parameter value; Can’t delete non-existing Rate Match Pattern " be shown.

Re-index will be done for the left Rate Match Pattern.

Initial S/W Revision

A.09.00

Copy Pattern

Copies the currently selected RateMatchPattern row with it's values and adds it to the table. The maximum number of supported BWPs is 8.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) >Ellipsis icon > Copy

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern:COPY <integer>

SCPI Example

 

Couplings

If count of Rate Match Pattern is 8 and try to copy Rate Match Pattern, error -224 "Illegal parameter value; Failed to copy Rate Match Pattern because limit of 8 has been reached." will be shown.

Initial S/W Revision

A.09.00

RateMatchPattern Count

Returns the number of RateMatchPattern(s). You can also see the number of pattern rows in the GUI.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s )

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern:COUNt?

SCPI Example

 

Preset

1

State Saved

No

Initial S/W Revision

A.09.00

ID

Display the ID of RateMatchPattern, it is automatically generated based on the index of RateMatchPattern array.

Enabled

Enables the channel or signal in a radio frame. When enabled and the subcarrier spacing is same as the subcarrier spacing of DLSCH, the rate match pattern will be applied to DLSCH when channel coding.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > Enabled

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7[:STATe]?

SCPI Example

 

Preset

Off

State Saved

Yes

Initial S/W Revision

A.09.00

Level

Choices: BWP Level | Cell Level

Default: BWP Level

Selects the Level for RateMatchPattern.

For BWP Level, the RB Index is refer to PRB index inside the BWP.

For Cell Level, the RB Index is refer to the CRB index corresponding to the selected subcarrier spacing.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > Level

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:LEVel CELL|BWP

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:LEVel?

SCPI Example

 

Preset

BWP

State Saved

Yes

Initial S/W Revision

A.09.00

Subcarrier Spacing

Choices:

BWP Level: Same as Subcarrier Spacing of the BWP of DLSCH

Cell Level: 15 kHz | 30kHz | 60kHz for FR1, 60 kHz | 120kHz for FR2

Select the Subcarrier Spacing for RateMatchPattern.

When Level is set to BWP, the subcarrier spacing is always set to the SCS of the associated BWP (default = 30 kHz). When Level is set to Cell Level, the subcarrier spacing is selectable as 15 kHz, 30 kHz or 60 kHz (FR1), and 60 kHz or 120 kHz (FR2). See TS 38.331 V16.1.0 for more information.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > Subcarrier Spacing

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:SCSPacing SCS15K|SCS30K|SCS60K|SCS120K

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:SCSPacing?

SCPI Example

 

Preset

SCS30K (30 kHz)

State Saved

Yes

Initial S/W Revision

A.09.00

RB Index

Range:

For BWP Level, RB Index is referred to PRB index inside the BWP, the range is 0 ~ (BWP.RBNumber - 1)

For Cell Level, the range of RB Index is 0 ~ N_grid_start[mu] + N_grid_size[mu] - 1, i.e. the length of RB Bitmap is N_grid_start[mu] + N_grid_size[mu]

If the selected numerology is not enabled, the range of RB Index is 0 ~ 274

Defines the resource blocks (RB) to which the rate match is applied. If an RB's index is included in the RB Index field, the rate match is applied to that resource block. See TS 38.331 V16.1.0 for more information. RBs are entered as an array of resource block indexes. There are 3 ways to configure:

These 3 configuration methods can be used in combination, by using ',' as the delimiter, e.g. 0,1,4:7,8:2:19 means index 0,1,4,5,6,7,8,10,12,14,16,18.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > RB Index

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:RB:INDex <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:RB:INDex?

SCPI Example

 

Preset

0:272

State Saved

Yes

Initial S/W Revision

A.09.00

Symbol Bitmap Span

Choices: OneSlot | TwoSlots

Default: OneSlot

Select the Symbol Bitmap Span for RateMatchPattern. Indicate the length of symbol bitmap, OneSlot means 14 bits, TwoSlots means 28 bits, no matter normal CP or extended CP.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > Symbol Bitmap Span

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:SBSPan ONE|TWO

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:SBSPan?

SCPI Example

 

Preset

One

State Saved

Yes

Initial S/W Revision

A.09.00

Symbol Bitmap

Default: 00000000000000

Enter a one-zero string to set the Symbol Bitmap, the length of this bitmap is equal to 14 for OneSlot, or 28 for TwoSlots. It indicates with a bit set to true that the UE shall rate match around the corresponding symbol. For Extended CP, the last two bits for OneSlot or the last four bits for TwoSlots are ignored.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > Symbol Bitmap

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:SBITmap <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:SBITmap?

SCPI Example

 

Preset

00000000000000

State Saved

Yes

Initial S/W Revision

A.09.00

Periodicity

Choices: 1 | 2 | 4 | 5 | 8 | 10 | 20 | 40

Default: 1

Select the Periodicity for Symbol Bitmap. It is the periodicity of Symbol Bitmap, for each period, the 'Periodicity Pattern Bitmap' is used to indicate which unit is rate matched.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > Periodicity

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:PERiodicity <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:PERiodicity?

SCPI Example

 

Preset

1

State Saved

Yes

Initial S/W Revision

A.09.00

Periodicity Pattern Bitmap

Default: 1

Enter an one-zero string to set the Periodicity Pattern Bitmap, the length of this bitmap is equal to Periodicity.

Each bit of 'Periodicity Pattern Bitmap' corresponds to a unit equal to a duration of the symbol level bitmap, and a bit value equal to 1 indicates that the pair is present in the unit.

GUI Location

Apps > 5G NR > Carrier > DL > Downlink > DL-SCH > RateMatchPattern(s) > Periodicity Pattern Bitmap

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:PPBitmap <string>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:DLINk:SCH<channel>:RMPattern0|1|2|3|4|5|6|7:PPBitmap?

SCPI Example

 

Preset

1

State Saved

Yes

Initial S/W Revision

A.09.00

Channel Setup DL-SCH